2.6 USB HID Device Library

Topics

Name Description
IntroductionIntroduces the MPLAB Harmony USB Human Interface Device (HID) Device Library.
Using the LibraryThis topic describes the basic architecture of the HID Function Driver and provides information and examples on its use.
Configuring the LibraryDescribes how to configure the HID Function Driver.
Library InterfaceThis section describes the Application Programming Interface (API) functions of the USB Device HID library.Refer to each section for a detailed description.
FilesThis section lists the source and header files used by the library.