1.3.2.4 CI/CD Wizard Dialog 4

Check to enable MISRA C verification. For more on MISRA, go to www.misra.org.uk/.

Requirements for using this features are:

  • A Jenkins plugin is required for either report selection. An informational note will provide a link.
  • MISRA C verification is only available for MPLAB X IDE v6.00 and later. An informational note will be displayed if the version does not support this feature.
Figure 1-5. Warnings Next Generation
OptionDescription
Enable MISRA-C VerificationCheck to enable MISRA verification.
Report PluginSelect from:
Informational Note (conditional)Depending on the plugin chosen, a note about the plugin will be displayed.