1.3.2.6 CI/CD Wizard Dialog 6

Check to enable a hardware tool for use as a test image and specify other options. This can be used to run unit tests.

A Microchip Debugger (MDB) script mdb-hardware-script.txt will be added to your project and this is executed during the hardware build step.

The default script will run for 10 seconds and capture output and coverage based on your settings. To change this, modify the script manually or regenerate using other options. Customize the input file as needed to fit your testing needs. Refer to the Microchip Debugger (MDB) User’s Guide.

Figure 1-7. Hardware Testing
OptionDescription
Enable Hardware TestingEnable hardware selection for testing
Tool to run test onEnable a debugger/emulator as a test tool.
Configuration to Build and Run on toolSelect a project configuration that uses the test tool; either default or one dedicated to hardware use.
IP Address of toolEnter the IP address of the tool you wish to use. If you do not know the IP address of the tool, you can open Tools > Manage Network Tools and scan for network tools. This will list the tool with its IP address.
Enable MPLAB Code CoverageEnable the MPLAB Code Coverage feature.
Note: The Code Coverage API plugin must be available on your Jenkins server if coverage reporting is enabled.
Scan Output for Unity Test ResultsEnable if the configuration builds Unity test runners, and the build job should create a report based on the resulting output. For more info on how to write Unity tests see How to Write and Run Unit Tests with Unity.