8.2 Debugger Options Selection
Debugger options are set in the Project Properties dialog. Click on ICD4, under Categories, to display Options for ICD4 (see figure below). Use the Option categories drop-down list to select various options. Click on an option name to see its description in the Option Description box below. Click to the right of an option name to select or change it.
After setting the options, click Apply or OK. Also click the
Refresh Debug Tool status icon
in the MPLAB X
IDE
dashboard display to update any changes made.
The possible option categories are described in the following sections.