Use of the SLEEP
instruction can allow an application to reduce its power comsumption considerably. AVR devices can be put into different sleep modes. Refer to the datasheet for the details relating to the device you are using.
There are several macros provided in this header file to actually put the device into sleep mode. The simplest way is to optionally set the desired sleep mode using set_sleep_mode()
(it usually defaults to idle mode where the CPU is put on sleep but all peripheral clocks are still running), and then call sleep_mode()
. This macro automatically sets the sleep enable bit, goes to sleep, and clears the sleep enable bit.
#include <avr/sleep.h> ... set_sleep_mode(<mode>); sleep_mode();
Note that unless your purpose is to completely lock the CPU (until a hardware reset), interrupts need to be enabled before going to sleep.
As the sleep_mode()
macro might cause race conditions in some situations, the individual steps of manipulating the sleep enable (SE) bit, and actually issuing the SLEEP
instruction, are provided in the macros sleep_enable()
, sleep_disable()
, and sleep_cpu()
. This also allows for test-and-sleep scenarios that take care of not missing the interrupt that will awake the device from sleep.
#include <avr/interrupt.h> #include <avr/sleep.h> ... set_sleep_mode(<mode>); cli(); if (some_condition) { sleep_enable(); sei(); sleep_cpu(); sleep_disable(); } sei();
This sequence ensures an atomic test of some_condition
with interrupts being disabled. If the condition is met, sleep mode will be prepared, and the SLEEP
instruction will be scheduled immediately after an SEI
instruction. As the intruction right after the SEI
is guaranteed to be executed before an interrupt could trigger, it is sure the device will really be put to sleep.
Some devices have the ability to disable the Brown Out Detector (BOD) before going to sleep. This will also reduce power while sleeping. If the specific AVR device has this ability then an additional macro is defined: sleep_bod_disable()
. This macro generates inlined assembly code that will correctly implement the timed sequence for disabling the BOD before sleeping. However, there is a limited number of cycles after the BOD has been disabled that the device can be put into sleep mode, otherwise the BOD will not truly be disabled. Recommended practice is to disable the BOD (sleep_bod_disable()
), set the interrupts (sei()
), and then put the device to sleep (sleep_cpu()
), like so:
#include <avr/interrupt.h> #include <avr/sleep.h> ... set_sleep_mode(<mode>); cli(); if (some_condition) { sleep_enable(); sleep_bod_disable(); sei(); sleep_cpu(); sleep_disable(); } sei();