This header file defines a debugging aid.
As there is no standard error output stream available for many applications using this library, the generation of a printable error message is not enabled by default. These messages will only be generated if the application defines the macro
before including the <assert.h>
header file. By default, only abort() will be called to halt the application.