This is a short summary of the AVR-specific aspects of using
the GNU tools. Normally, the generic documentation of these tools is fairly
large and maintained in texinfo
files. Command-line options
are explained in detail in the manual page.
Machine-specific options for the AVR
The following machine-specific options are recognized by the C compiler frontend. In addition to the preprocessor macros indicated in the tables below, the preprocessor will define the macros __AVR and __AVR__ (to the value 1) when compiling for an AVR target. The macro AVR will be defined as well when using the standard levels gnu89 (default) and gnu99 but not with c89 and c99.
-mmcu=
architecture
Compile code for architecture. Currently known architectures are
Architecture |
Macros |
Description |
---|---|---|
avr1 |
__AVR_ARCH__=1 __AVR_ASM_ONLY__ __AVR_2_BYTE_PC__ [2] |
Simple CPU core, only assembler support |
avr2 |
__AVR_ARCH__=2 __AVR_2_BYTE_PC__ [2] |
"Classic" CPU core, up to 8 KB of ROM |
avr25 [1] |
__AVR_ARCH__=25 __AVR_HAVE_MOVW__ [1] __AVR_HAVE_LPMX__ [1] __AVR_2_BYTE_PC__ [2] |
"Classic" CPU core with 'MOVW' and 'LPM Rx, Z[+]' instruction, up to 8 KB of ROM |
avr3 |
__AVR_ARCH__=3 __AVR_MEGA__ [5] __AVR_HAVE_JMP_CALL__ [4] __AVR_2_BYTE_PC__ [2] |
"Classic" CPU core, 16 KB to 64 KB of ROM |
avr31 |
__AVR_ARCH__=31 __AVR_MEGA__ [5] __AVR_HAVE_JMP_CALL__ [4] __AVR_HAVE_RAMPZ__ [4] __AVR_HAVE_ELPM__ [4] __AVR_2_BYTE_PC__ [2] |
"Classic" CPU core, 128 KB of ROM |
avr35 [3] |
__AVR_ARCH__=35 __AVR_MEGA__ [5] __AVR_HAVE_JMP_CALL__ [4] __AVR_HAVE_MOVW__ [1] __AVR_HAVE_LPMX__ [1] __AVR_2_BYTE_PC__ [2] |
"Classic" CPU core with 'MOVW' and 'LPM Rx, Z[+]' instruction, 16 KB to 64 KB of ROM |
avr4 |
__AVR_ARCH__=4 __AVR_ENHANCED__ [5] __AVR_HAVE_MOVW__ [1] __AVR_HAVE_LPMX__ [1] __AVR_HAVE_MUL__ [1] __AVR_2_BYTE_PC__ [2] |
"Enhanced" CPU core, up to 8 KB of ROM |
avr5 |
__AVR_ARCH__=5 __AVR_MEGA__ [5] __AVR_ENHANCED__ [5] __AVR_HAVE_JMP_CALL__ [4] __AVR_HAVE_MOVW__ [1] __AVR_HAVE_LPMX__ [1] __AVR_HAVE_MUL__ [1] __AVR_2_BYTE_PC__ [2] |
"Enhanced" CPU core, 16 KB to 64 KB of ROM |
avr51 |
__AVR_ARCH__=51 __AVR_MEGA__ [5] __AVR_ENHANCED__ [5] __AVR_HAVE_JMP_CALL__ [4] __AVR_HAVE_MOVW__ [1] __AVR_HAVE_LPMX__ [1] __AVR_HAVE_MUL__ [1] __AVR_HAVE_RAMPZ__ [4] __AVR_HAVE_ELPM__ [4] __AVR_HAVE_ELPMX__ [4] __AVR_2_BYTE_PC__ [2] |
"Enhanced" CPU core, 128 KB of ROM |
avr6 [2] |
__AVR_ARCH__=6 __AVR_MEGA__ [5] __AVR_ENHANCED__ [5] __AVR_HAVE_JMP_CALL__ [4] __AVR_HAVE_MOVW__ [1] __AVR_HAVE_LPMX__ [1] __AVR_HAVE_MUL__ [1] __AVR_HAVE_RAMPZ__ [4] __AVR_HAVE_ELPM__ [4] __AVR_HAVE_ELPMX__ [4] __AVR_3_BYTE_PC__ [2] |
"Enhanced" CPU core, 256 KB of ROM |
[1] New in GCC 4.2 [2] Unofficial patch for GCC 4.1 [3] New in GCC 4.2.3 [4] New in GCC 4.3 [5] Obsolete.
By default, code is generated for the avr2 architecture.
Note that when only using
-mmcu=
architecture but no
-mmcu=
MCU type, including the file
<avr/io.h>
cannot work since
it cannot decide which device's definitions to select.
-mmcu=
MCU type
The following MCU types are currently understood by avr-gcc.
The table matches them against the corresponding avr-gcc architecture name,
and shows the preprocessor symbol declared by the -mmcu
option.
Architecture |
MCU name |
Macro |
---|---|---|
avr1 |
at90s1200 |
__AVR_AT90S1200__ |
avr1 |
attiny11 |
__AVR_ATtiny11__ |
avr1 |
attiny12 |
__AVR_ATtiny12__ |
avr1 |
attiny15 |
__AVR_ATtiny15__ |
avr1 |
attiny28 |
__AVR_ATtiny28__ |
avr2 |
at90s2313 |
__AVR_AT90S2313__ |
avr2 |
at90s2323 |
__AVR_AT90S2323__ |
avr2 |
at90s2333 |
__AVR_AT90S2333__ |
avr2 |
at90s2343 |
__AVR_AT90S2343__ |
avr2 |
attiny22 |
__AVR_ATtiny22__ |
avr2 |
attiny26 |
__AVR_ATtiny26__ |
avr2 |
at90s4414 |
__AVR_AT90S4414__ |
avr2 |
at90s4433 |
__AVR_AT90S4433__ |
avr2 |
at90s4434 |
__AVR_AT90S4434__ |
avr2 |
at90s8515 |
__AVR_AT90S8515__ |
avr2 |
at90c8534 |
__AVR_AT90C8534__ |
avr2 |
at90s8535 |
__AVR_AT90S8535__ |
avr2/avr25 [1] |
at86rf401 |
__AVR_AT86RF401__ |
avr2/avr25 [1] |
ata5272 |
__AVR_ATA5272__ |
avr2/avr25 [1] |
ata6616c |
__AVR_ATA6616C__ |
avr2/avr25 [1] |
attiny13 |
__AVR_ATtiny13__ |
avr2/avr25 [1] |
attiny13a |
__AVR_ATtiny13A__ |
avr2/avr25 [1] |
attiny2313 |
__AVR_ATtiny2313__ |
avr2/avr25 [1] |
attiny2313a |
__AVR_ATtiny2313A__ |
avr2/avr25 [1] |
attiny24 |
__AVR_ATtiny24__ |
avr2/avr25 [1] |
attiny24a |
__AVR_ATtiny24A__ |
avr2/avr25 [1] |
attiny25 |
__AVR_ATtiny25__ |
avr2/avr25 [1] |
attiny261 |
__AVR_ATtiny261__ |
avr2/avr25 [1] |
attiny261a |
__AVR_ATtiny261A__ |
avr2/avr25 [1] |
attiny4313 |
__AVR_ATtiny4313__ |
avr2/avr25 [1] |
attiny43u |
__AVR_ATtiny43U__ |
avr2/avr25 [1] |
attiny44 |
__AVR_ATtiny44__ |
avr2/avr25 [1] |
attiny44a |
__AVR_ATtiny44A__ |
avr2/avr25 [1] |
attiny441 |
__AVR_ATtiny441__ |
avr2/avr25 [1] |
attiny45 |
__AVR_ATtiny45__ |
avr2/avr25 [1] |
attiny461 |
__AVR_ATtiny461__ |
avr2/avr25 [1] |
attiny461a |
__AVR_ATtiny461A__ |
avr2/avr25 [1] |
attiny48 |
__AVR_ATtiny48__ |
avr2/avr25 [1] |
attiny828 |
__AVR_ATtiny828__ |
avr2/avr25 [1] |
attiny84 |
__AVR_ATtiny84__ |
avr2/avr25 [1] |
attiny84a |
__AVR_ATtiny84A__ |
avr2/avr25 [1] |
attiny841 |
__AVR_ATtiny841__ |
avr2/avr25 [1] |
attiny85 |
__AVR_ATtiny85__ |
avr2/avr25 [1] |
attiny861 |
__AVR_ATtiny861__ |
avr2/avr25 [1] |
attiny861a |
__AVR_ATtiny861A__ |
avr2/avr25 [1] |
attiny87 |
__AVR_ATtiny87__ |
avr2/avr25 [1] |
attiny88 |
__AVR_ATtiny88__ |
avr3 |
atmega603 |
__AVR_ATmega603__ |
avr3 |
at43usb355 |
__AVR_AT43USB355__ |
avr3/avr31 [3] |
atmega103 |
__AVR_ATmega103__ |
avr3/avr31 [3] |
at43usb320 |
__AVR_AT43USB320__ |
avr3/avr35 [2] |
at90usb82 |
__AVR_AT90USB82__ |
avr3/avr35 [2] |
at90usb162 |
__AVR_AT90USB162__ |
avr3/avr35 [2] |
ata5505 |
__AVR_ATA5505__ |
avr3/avr35 [2] |
ata6617c |
__AVR_ATA6617C__ |
avr3/avr35 [2] |
ata664251 |
__AVR_ATA664251__ |
avr3/avr35 [2] |
atmega8u2 |
__AVR_ATmega8U2__ |
avr3/avr35 [2] |
atmega16u2 |
__AVR_ATmega16U2__ |
avr3/avr35 [2] |
atmega32u2 |
__AVR_ATmega32U2__ |
avr3/avr35 [2] |
attiny167 |
__AVR_ATtiny167__ |
avr3/avr35 [2] |
attiny1634 |
__AVR_ATtiny1634__ |
avr3 |
at76c711 |
__AVR_AT76C711__ |
avr4 |
ata6285 |
__AVR_ATA6285__ |
avr4 |
ata6286 |
__AVR_ATA6286__ |
avr4 |
ata6289 |
__AVR_ATA6289__ |
avr4 |
ata6612c |
__AVR_ATA6612C__ |
avr4 |
atmega48 |
__AVR_ATmega48__ |
avr4 |
atmega48a |
__AVR_ATmega48A__ |
avr4 |
atmega48pa |
__AVR_ATmega48PA__ |
avr4 |
atmega48pb |
__AVR_ATmega48PB__ |
avr4 |
atmega48p |
__AVR_ATmega48P__ |
avr4 |
atmega8 |
__AVR_ATmega8__ |
avr4 |
atmega8a |
__AVR_ATmega8A__ |
avr4 |
atmega8515 |
__AVR_ATmega8515__ |
avr4 |
atmega8535 |
__AVR_ATmega8535__ |
avr4 |
atmega88 |
__AVR_ATmega88__ |
avr4 |
atmega88a |
__AVR_ATmega88A__ |
avr4 |
atmega88p |
__AVR_ATmega88P__ |
avr4 |
atmega88pa |
__AVR_ATmega88PA__ |
avr4 |
atmega88pb |
__AVR_ATmega88PB__ |
avr4 |
atmega8hva |
__AVR_ATmega8HVA__ |
avr4 |
at90pwm1 |
__AVR_AT90PWM1__ |
avr4 |
at90pwm2 |
__AVR_AT90PWM2__ |
avr4 |
at90pwm2b |
__AVR_AT90PWM2B__ |
avr4 |
at90pwm3 |
__AVR_AT90PWM3__ |
avr4 |
at90pwm3b |
__AVR_AT90PWM3B__ |
avr4 |
at90pwm81 |
__AVR_AT90PWM81__ |
avr5 |
at90can32 |
__AVR_AT90CAN32__ |
avr5 |
at90can64 |
__AVR_AT90CAN64__ |
avr5 |
at90pwm161 |
__AVR_AT90PWM161__ |
avr5 |
at90pwm216 |
__AVR_AT90PWM216__ |
avr5 |
at90pwm316 |
__AVR_AT90PWM316__ |
avr5 |
at90scr100 |
__AVR_AT90SCR100__ |
avr5 |
at90usb646 |
__AVR_AT90USB646__ |
avr5 |
at90usb647 |
__AVR_AT90USB647__ |
avr5 |
at94k |
__AVR_AT94K__ |
avr5 |
atmega16 |
__AVR_ATmega16__ |
avr5 |
ata5702m322 |
__AVR_ATA5702M322__ |
avr5 |
ata5782 |
__AVR_ATA5782__ |
avr5 |
ata5790 |
__AVR_ATA5790__ |
avr5 |
ata5790n |
__AVR_ATA5790N__ |
avr5 |
ata5791 |
__AVR_ATA5791__ |
avr5 |
ata5795 |
__AVR_ATA5795__ |
avr5 |
ata5831 |
__AVR_ATA5831__ |
avr5 |
ata6613c |
__AVR_ATA6613C__ |
avr5 |
ata6614q |
__AVR_ATA6614Q__ |
avr5 |
ata8210 |
__AVR_ATA8210__ |
avr5 |
ata8510 |
__AVR_ATA8510__ |
avr5 |
atmega161 |
__AVR_ATmega161__ |
avr5 |
atmega162 |
__AVR_ATmega162__ |
avr5 |
atmega163 |
__AVR_ATmega163__ |
avr5 |
atmega164a |
__AVR_ATmega164A__ |
avr5 |
atmega164p |
__AVR_ATmega164P__ |
avr5 |
atmega164pa |
__AVR_ATmega164PA__ |
avr5 |
atmega165 |
__AVR_ATmega165__ |
avr5 |
atmega165a |
__AVR_ATmega165A__ |
avr5 |
atmega165p |
__AVR_ATmega165P__ |
avr5 |
atmega165pa |
__AVR_ATmega165PA__ |
avr5 |
atmega168 |
__AVR_ATmega168__ |
avr5 |
atmega168a |
__AVR_ATmega168A__ |
avr5 |
atmega168p |
__AVR_ATmega168P__ |
avr5 |
atmega168pa |
__AVR_ATmega168PA__ |
avr5 |
atmega168pb |
__AVR_ATmega168PB__ |
avr5 |
atmega169 |
__AVR_ATmega169__ |
avr5 |
atmega169a |
__AVR_ATmega169A__ |
avr5 |
atmega169p |
__AVR_ATmega169P__ |
avr5 |
atmega169pa |
__AVR_ATmega169PA__ |
avr5 |
atmega16a |
__AVR_ATmega16A__ |
avr5 |
atmega16hva |
__AVR_ATmega16HVA__ |
avr5 |
atmega16hva2 |
__AVR_ATmega16HVA2__ |
avr5 |
atmega16hvb |
__AVR_ATmega16HVB__ |
avr5 |
atmega16hvbrevb |
__AVR_ATmega16HVBREVB__ |
avr5 |
atmega16m1 |
__AVR_ATmega16M1__ |
avr5 |
atmega16u4 |
__AVR_ATmega16U4__ |
avr5 |
atmega32 |
__AVR_ATmega32__ |
avr5 |
atmega32a |
__AVR_ATmega32A__ |
avr5 |
atmega323 |
__AVR_ATmega323__ |
avr5 |
atmega324a |
__AVR_ATmega324A__ |
avr5 |
atmega324p |
__AVR_ATmega324P__ |
avr5 |
atmega324pa |
__AVR_ATmega324PA__ |
avr5 |
atmega325 |
__AVR_ATmega325__ |
avr5 |
atmega325a |
__AVR_ATmega325A__ |
avr5 |
atmega325p |
__AVR_ATmega325P__ |
avr5 |
atmega325pa |
__AVR_ATmega325PA__ |
avr5 |
atmega3250 |
__AVR_ATmega3250__ |
avr5 |
atmega3250a |
__AVR_ATmega3250A__ |
avr5 |
atmega3250p |
__AVR_ATmega3250P__ |
avr5 |
atmega3250pa |
__AVR_ATmega3250PA__ |
avr5 |
atmega328 |
__AVR_ATmega328__ |
avr5 |
atmega328p |
__AVR_ATmega328P__ |
avr5 |
atmega329 |
__AVR_ATmega329__ |
avr5 |
atmega329a |
__AVR_ATmega329A__ |
avr5 |
atmega329p |
__AVR_ATmega329P__ |
avr5 |
atmega329pa |
__AVR_ATmega329PA__ |
avr5 |
atmega3290 |
__AVR_ATmega3290__ |
avr5 |
atmega3290a |
__AVR_ATmega3290A__ |
avr5 |
atmega3290p |
__AVR_ATmega3290P__ |
avr5 |
atmega3290pa |
__AVR_ATmega3290PA__ |
avr5 |
atmega32c1 |
__AVR_ATmega32C1__ |
avr5 |
atmega32hvb |
__AVR_ATmega32HVB__ |
avr5 |
atmega32hvbrevb |
__AVR_ATmega32HVBREVB__ |
avr5 |
atmega32m1 |
__AVR_ATmega32M1__ |
avr5 |
atmega32u4 |
__AVR_ATmega32U4__ |
avr5 |
atmega32u6 |
__AVR_ATmega32U6__ |
avr5 |
atmega406 |
__AVR_ATmega406__ |
avr5 |
atmega644rfr2 |
__AVR_ATmega644RFR2__ |
avr5 |
atmega64rfr2 |
__AVR_ATmega64RFR2__ |
avr5 |
atmega64 |
__AVR_ATmega64__ |
avr5 |
atmega64a |
__AVR_ATmega64A__ |
avr5 |
atmega640 |
__AVR_ATmega640__ |
avr5 |
atmega644 |
__AVR_ATmega644__ |
avr5 |
atmega644a |
__AVR_ATmega644A__ |
avr5 |
atmega644p |
__AVR_ATmega644P__ |
avr5 |
atmega644pa |
__AVR_ATmega644PA__ |
avr5 |
atmega645 |
__AVR_ATmega645__ |
avr5 |
atmega645a |
__AVR_ATmega645A__ |
avr5 |
atmega645p |
__AVR_ATmega645P__ |
avr5 |
atmega6450 |
__AVR_ATmega6450__ |
avr5 |
atmega6450a |
__AVR_ATmega6450A__ |
avr5 |
atmega6450p |
__AVR_ATmega6450P__ |
avr5 |
atmega649 |
__AVR_ATmega649__ |
avr5 |
atmega649a |
__AVR_ATmega649A__ |
avr5 |
atmega6490 |
__AVR_ATmega6490__ |
avr5 |
atmega6490a |
__AVR_ATmega6490A__ |
avr5 |
atmega6490p |
__AVR_ATmega6490P__ |
avr5 |
atmega649p |
__AVR_ATmega649P__ |
avr5 |
atmega64c1 |
__AVR_ATmega64C1__ |
avr5 |
atmega64hve |
__AVR_ATmega64HVE__ |
avr5 |
atmega64hve2 |
__AVR_ATmega64HVE2__ |
avr5 |
atmega64m1 |
__AVR_ATmega64M1__ |
avr5 |
m3000 |
__AVR_M3000__ |
avr5/avr51 [3] |
at90can128 |
__AVR_AT90CAN128__ |
avr5/avr51 [3] |
at90usb1286 |
__AVR_AT90USB1286__ |
avr5/avr51 [3] |
at90usb1287 |
__AVR_AT90USB1287__ |
avr5/avr51 [3] |
atmega128 |
__AVR_ATmega128__ |
avr5/avr51 [3] |
atmega128a |
__AVR_ATmega128A__ |
avr5/avr51 [3] |
atmega1280 |
__AVR_ATmega1280__ |
avr5/avr51 [3] |
atmega1281 |
__AVR_ATmega1281__ |
avr5/avr51 [3] |
atmega1284 |
__AVR_ATmega1284__ |
avr5/avr51 [3] |
atmega1284p |
__AVR_ATmega1284P__ |
avr5/avr51 [3] |
atmega1284rfr2 |
__AVR_ATmega1284RFR2__ |
avr5/avr51 [3] |
atmega128rfr2 |
__AVR_ATmega128RFR2__ |
avr6 |
atmega2560 |
__AVR_ATmega2560__ |
avr6 |
atmega2561 |
__AVR_ATmega2561__ |
avr6 |
atmega2564rfr2 |
__AVR_ATmega2564RFR2__ |
avr6 |
atmega256rfr2 |
__AVR_ATmega256RFR2__ |
avrxmega2 |
atxmega8e5 |
__AVR_ATxmega8E5__ |
avrxmega2 |
atxmega16a4 |
__AVR_ATxmega16A4__ |
avrxmega2 |
atxmega16a4u |
__AVR_ATxmega16A4U__ |
avrxmega2 |
atxmega16c4 |
__AVR_ATxmega16C4__ |
avrxmega2 |
atxmega16d4 |
__AVR_ATxmega16D4__ |
avrxmega2 |
atxmega16e5 |
__AVR_ATxmega16E5__ |
avrxmega2 |
atxmega32a4 |
__AVR_ATxmega32A4__ |
avrxmega2 |
atxmega32a4u |
__AVR_ATxmega32A4U__ |
avrxmega2 |
atxmega32c3 |
__AVR_ATxmega32C3__ |
avrxmega2 |
atxmega32c4 |
__AVR_ATxmega32C4__ |
avrxmega2 |
atxmega32d3 |
__AVR_ATxmega32D3__ |
avrxmega2 |
atxmega32d4 |
__AVR_ATxmega32D4__ |
avrxmega2 |
atxmega32e5 |
__AVR_ATxmega32E5__ |
avrxmega4 |
atxmega64a3 |
__AVR_ATxmega64A3__ |
avrxmega4 |
atxmega64a3u |
__AVR_ATxmega64A3U__ |
avrxmega4 |
atxmega64a4u |
__AVR_ATxmega64A4U__ |
avrxmega4 |
atxmega64b1 |
__AVR_ATxmega64B1__ |
avrxmega4 |
atxmega64b3 |
__AVR_ATxmega64B3__ |
avrxmega4 |
atxmega64c3 |
__AVR_ATxmega64C3__ |
avrxmega4 |
atxmega64d3 |
__AVR_ATxmega64D3__ |
avrxmega4 |
atxmega64d4 |
__AVR_ATxmega64D4__ |
avrxmega5 |
atxmega64a1 |
__AVR_ATxmega64A1__ |
avrxmega5 |
atxmega64a1u |
__AVR_ATxmega64A1U__ |
avrxmega6 |
atxmega128a3 |
__AVR_ATxmega128A3__ |
avrxmega6 |
atxmega128a3u |
__AVR_ATxmega128A3U__ |
avrxmega6 |
atxmega128b1 |
__AVR_ATxmega128B1__ |
avrxmega6 |
atxmega128b3 |
__AVR_ATxmega128B3__ |
avrxmega6 |
atxmega128c3 |
__AVR_ATxmega128C3__ |
avrxmega6 |
atxmega128d3 |
__AVR_ATxmega128D3__ |
avrxmega6 |
atxmega128d4 |
__AVR_ATxmega128D4__ |
avrxmega6 |
atxmega192a3 |
__AVR_ATxmega192A3__ |
avrxmega6 |
atxmega192a3u |
__AVR_ATxmega192A3U__ |
avrxmega6 |
atxmega192c3 |
__AVR_ATxmega192C3__ |
avrxmega6 |
atxmega192d3 |
__AVR_ATxmega192D3__ |
avrxmega6 |
atxmega256a3 |
__AVR_ATxmega256A3__ |
avrxmega6 |
atxmega256a3u |
__AVR_ATxmega256A3U__ |
avrxmega6 |
atxmega256a3b |
__AVR_ATxmega256A3B__ |
avrxmega6 |
atxmega256a3bu |
__AVR_ATxmega256A3BU__ |
avrxmega6 |
atxmega256c3 |
__AVR_ATxmega256C3__ |
avrxmega6 |
atxmega256d3 |
__AVR_ATxmega256D3__ |
avrxmega6 |
atxmega384c3 |
__AVR_ATxmega384C3__ |
avrxmega6 |
atxmega384d3 |
__AVR_ATxmega384D3__ |
avrxmega7 |
atxmega128a1 |
__AVR_ATxmega128A1__ |
avrxmega7 |
atxmega128a1u |
__AVR_ATxmega128A1U__ |
avrxmega7 |
atxmega128a4u |
__AVR_ATxmega128A4U__ |
avrtiny10 |
attiny4 |
__AVR_ATtiny4__ |
avrtiny10 |
attiny5 |
__AVR_ATtiny5__ |
avrtiny10 |
attiny9 |
__AVR_ATtiny9__ |
avrtiny10 |
attiny10 |
__AVR_ATtiny10__ |
avrtiny10 |
attiny20 |
__AVR_ATtiny20__ |
avrtiny10 |
attiny40 |
__AVR_ATtiny40__ |
[1] 'avr25' architecture is new in GCC 4.2 [2] 'avr35' architecture is new in GCC 4.2.3 [3] 'avr31' and 'avr51' architectures is new in GCC 4.3
-morder1
-morder2
Change the order of register assignment. The default is
r24, r25, r18, r19, r20, r21, r22, r23, r30, r31, r26, r27, r28, r29, r17, r16, r15, r14, r13, r12, r11, r10, r9, r8, r7, r6, r5, r4, r3, r2, r0, r1
Order 1 uses
r18, r19, r20, r21, r22, r23, r24, r25, r30, r31, r26, r27, r28, r29, r17, r16, r15, r14, r13, r12, r11, r10, r9, r8, r7, r6, r5, r4, r3, r2, r0, r1
Order 2 uses
r25, r24, r23, r22, r21, r20, r19, r18, r30, r31, r26, r27, r28, r29, r17, r16, r15, r14, r13, r12, r11, r10, r9, r8, r7, r6, r5, r4, r3, r2, r1, r0
-mint8
Assume int
to be an 8-bit integer. Note that
this is not really supported by avr-libc
, so it should
normally not be used. The default is to use 16-bit integers.
-mno-interrupts
Generates code that changes the stack pointer without
disabling interrupts. Normally, the state of the status register
SREG
is saved in a temporary register, interrupts are
disabled while changing the stack pointer, and SREG
is
restored.
Specifying this option will define the preprocessor macro
__NO_INTERRUPTS__
to the value 1.
-mcall-prologues
Use subroutines for function prologue/epilogue. For complex functions that use many registers (that needs to be saved/restored on function entry/exit), this saves some space at the cost of a slightly increased execution time.
-mtiny-stack
Change only the low 8 bits of the stack pointer.
-mno-tablejump
Deprecated, use -fno-jump-tables
instead.
-mshort-calls
Use rjmp/rcall
(limited range) on >8K
devices. On avr2
and avr4
architectures
(less than 8 KB or flash memory), this is always the case. On
avr3
and avr5
architectures, calls and
jumps to targets outside the current function will by default use
jmp/call
instructions that can cover the entire address
range, but that require more flash ROM and execution time.
-mrtl
Dump the internal compilation result called "RTL" into comments in the generated assembler code. Used for debugging avr-gcc.
-msize
Dump the address, size, and relative cost of each statement into comments in the generated assembler code. Used for debugging avr-gcc.
-mdeb
Generate lots of debugging information to
stderr
.
Selected general compiler options
The following general gcc options might be of some interest to AVR users.
-O
n
Optimization level n. Increasing n is meant to
optimize more, an optimization level of 0 means no optimization at all,
which is the default if no -O
option is present. The
special option -Os
is meant to turn on all
-O2
optimizations that are not expected to increase code
size.
Note that at -O3
, gcc attempts to inline all
"simple" functions. For the AVR target, this will normally constitute a
large pessimization due to the code increasement. The only other
optimization turned on with -O3
is
-frename-registers
, which could rather be enabled manually
instead.
A simple -O
option is equivalent to
-O1
.
Note also that turning off all optimizations will prevent some warnings from being issued since the generation of those warnings depends on code analysis steps that are only performed when optimizing (unreachable code, unused variables).
-Wa,
assembler-options
-Wl,
linker-options
Pass the listed options to the assembler, or linker, respectively.
-g
Generate debugging information that can be used by avr-gdb.
-ffreestanding
Assume a "freestanding" environment as per the C standard.
This turns off automatic builtin functions (though they can still be reached
by prepending __builtin_
to the actual function name). It
also makes the compiler not complain when main()
is
declared with a void
return type which makes some sense in
a microcontroller environment where the application cannot meaningfully
provide a return value to its environment (in most cases,
main()
won't even return anyway). However, this also turns
off all optimizations normally done by the compiler which assume that
functions known by a certain name behave as described by the standard. E.
g., applying the function strlen() to a literal string will
normally cause the compiler to immediately replace that call by the actual
length of the string, while with -ffreestanding
, it will
always call strlen() at run-time.
-funsigned-char
Make any unqualfied char
type an unsigned
char. Without this option, they default to a signed char.
-funsigned-bitfields
Make any unqualified bitfield type unsigned. By default, they are signed.
-fshort-enums
Allocate to an enum
type only as many bytes
as it needs for the declared range of possible values. Specifically, the
enum type will be equivalent to the smallest integer type which has enough
room.
-fpack-struct
Pack all structure members together without holes.
-fno-jump-tables
Do not generate tablejump instructions. By default, jump
tables can be used to optimize switch
statements. When
turned off, sequences of compare statements are used instead. Jump tables
are usually faster to execute on average, but in particular for
switch
statements, where most of the jumps would go to the
default label, they might waste a bit of flash memory.
NOTE: The tablejump instructions use the LPM assembler
instruction for access to jump tables. Always use
-fno-jump-tables
switch, if compiling a bootloader for
devices with more than 64 KB of code memory.
Machine-specific assembler options
-mmcu=
architecture
-mmcu=
MCU name
avr-as understands the same -mmcu=
options
as avr-gcc. By default, avr2 is assumed, but
this can be altered by using the appropriate .arch pseudo-instruction inside
the assembler source file.
-mall-opcodes
Turns off opcode checking for the actual MCU type, and allows any possible AVR opcode to be assembled.
-mno-skip-bug
Don't emit a warning when trying to skip a 2-word instruction
with a CPSE/SBIC/SBIS/SBRC/SBRS
instruction. Early AVR
devices suffered from a hardware bug where these instructions could not be
properly skipped.
-mno-wrap
For RJMP/RCALL
instructions, don't allow the
target address to wrap around for devices that have more than 8 KB of
memory.
--gstabs
Generate .stabs debugging symbols for assembler
source lines. This enables avr-gdb to trace through assembler source files.
This option must not be used when assembling sources that have been
generated by the C compiler; these files already contain the appropriate
line number information from the C source files.
-a[cdhlmns=
file]
Turn on the assembler listing. The sub-options are:
c
omit false conditionals
d
omit debugging directives
h
include high-level source
l
include assembly
m
include macro expansions
n
omit forms processing
s
include symbols
=
file set the name of the listing
file
The various sub-options can be combined into a single
-a
option list; =file must be the last one in that
case.
Examples for assembler options passed through the C compiler
Remember that assembler options can be passed from the C
compiler frontend using -Wa
(see above), so in order to include the C
source code into the assembler listing in file foo.lst
,
when compiling foo.c
, the following compiler command-line
can be used:
In order to pass an assembler file through the C preprocessor first, and have the assembler generate line number debugging information for it, the following command can be used:
Note that on Unix systems that have case-distinguishing file
systems, specifying a file name with the suffix .S (upper-case
letter S) will make the compiler automatically assume
-x
assembler-with-cpp
, while using .s would pass the file
directly to the assembler (no preprocessing done).
Selected linker options
While there are no machine-specific options for avr-ld, a number of the standard options might be of interest to AVR users.
-l
name
Locate the archive library named
lib
name.a
, and use it to resolve
currently unresolved symbols from it. The library is searched along a path
that consists of builtin pathname entries that have been specified at
compile time (e. g. /usr/local/avr/lib
on Unix systems),
possibly extended by pathname entries as specified by -L
options (that must precede the -l
options on the
command-line).
-L
path
Additional location to look for archive libraries requested by
-l
options.
--defsym
symbol=expr
Define a global symbol symbol using expr as the value.
-M
Print a linker map to stdout
.
-Map
mapfile
Print a linker map to mapfile.
--cref
Output a cross reference table to the map file (in case
-Map
is also present), or to stdout
.
--section-start
sectionname=org
Start section sectionname at absolute address org.
-Tbss
org
-Tdata
org
-Ttext
org
Start the bss
, data
, or
text
section at org, respectively.
-T
scriptfile
Use scriptfile as the linker script, replacing the
default linker script. Default linker scripts are stored in a
system-specific location (e. g. under
/usr/local/avr/lib/ldscripts
on Unix systems), and consist
of the AVR architecture name (avr2 through avr5) with the suffix .x
appended. They describe how the various memory sections will be linked together.
Passing linker options from the C compiler
By default, all unknown non-option arguments on the avr-gcc
command-line (i. e., all filename arguments that don't have a suffix that is
handled by avr-gcc) are passed straight to the linker. Thus, all files
ending in .o (object files) and
.a (object libraries) are
provided to the linker.
System libraries are usually not passed by their explicit
filename but rather using the -l
option which uses an
abbreviated form of the archive filename (see above). avr-libc ships two
system libraries, libc.a
, and libm.a
.
While the standard library libc.a
will always be searched
for unresolved references when the linker is started using the C compiler
frontend (i. e., there's always at least one implied -lc
option), the mathematics library libm.a
needs to be
explicitly requested using -lm
. See also the entry in the FAQ explaining this.
Conventionally, Makefiles use the make
macro
LDLIBS
to keep track of -l
(and possibly
-L
) options that should only be appended to the C compiler
command-line when linking the final binary. In contrast, the macro
LDFLAGS
is used to store other command-line options to the
C compiler that should be passed as options during the linking stage. The
difference is that options are placed early on the command-line, while
libraries are put at the end since they are to be used to resolve global
symbols that are still unresolved at this point.
Specific linker flags can be passed from the C compiler
command-line using the -Wl
compiler option, see above. This option requires that there be
no spaces in the appended linker option, while some of the linker options
above (like -Map
or --defsym
) would
require a space. In these situations, the space can be replaced by an equal
sign as well. For example, the following command-line can be used to compile
foo.c
into an executable, and also produce a link map that
contains a cross-reference list in the file foo.map:
Alternatively, a comma as a placeholder will be replaced by a space before passing the option to the linker. So for a device with external SRAM, the following command-line would cause the linker to place the data segment at address 0x2000 in the SRAM:
See the explanation of the data section for why 0x800000 needs to be
added to the actual value. Note that the stack will still remain in internal
RAM, through the symbol __stack
that is provided by the
run-time startup code. This is probably a good idea anyway (since internal
RAM access is faster), and even required for some early devices that had
hardware bugs preventing them from using a stack in external RAM. Note also
that the heap for malloc()
will still be placed
after all the variables in the data section, so in this situation, no
stack/heap collision can occur.
In order to relocate the stack from its default location at
the top of interns RAM, the value of the symbol __stack
can
be changed on the linker command-line. As the linker is typically called
from the compiler frontend, this can be achieved using a compiler option
like
The above will make the code use stack space from RAM address 0x3ff downwards. The amount of stack space available then depends on the bottom address of internal RAM for a particular device. It is the responsibility of the application to ensure the stack does not grow out of bounds, as well as to arrange for the stack to not collide with variable allocations made by the compiler (sections .data and .bss).