char * strchr(const char *, int) __ATTR_PURE__
The strchr() function returns a pointer to the first occurrence of the character val
in the string src
.
Here "character" means "byte" - these functions do not work with wide or multi-byte characters.
The strchr() function returns a pointer to the matched character or NULL
if the character is not found.