char * strpbrk(const char *__s, const char *__accept) __ATTR_PURE__
The strpbrk() function locates the first occurrence in the string s
of any of the characters in the string accept
.
The strpbrk() function returns a pointer to the character in s
that matches one of the characters in accept
, or NULL
if no such character is found. The terminating zero is not considered as a part of string: if one or both args are empty, the result will be NULL
.