char * strcasestr(const char *, const char *) __ATTR_PURE__
The strcasestr() function finds the first occurrence of the substring s2
in the string s1
. This is like strstr(), except that it ignores case of alphabetic symbols in searching for the substring. (Glibc, GNU extension.)
The strcasestr() function returns a pointer to the beginning of the substring, or NULL
if the substring is not found. If s2
points to a string of zero length, the function returns s1
.