atoi.S

/* Copyright (c) 2002, 2007 Reiner Patommel
   All rights reserved.

   Redistribution and use in source and binary forms, with or without
   modification, are permitted provided that the following conditions are met:

   * Redistributions of source code must retain the above copyright
     notice, this list of conditions and the following disclaimer.
   * Redistributions in binary form must reproduce the above copyright
     notice, this list of conditions and the following disclaimer in
     the documentation and/or other materials provided with the
     distribution.
   * Neither the name of the copyright holders nor the names of
     contributors may be used to endorse or promote products derived
     from this software without specific prior written permission.

  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
  AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
  IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
  ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
  LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
  CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
  SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
  INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
  CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
  ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
  POSSIBILITY OF SUCH DAMAGE. */  

/* $Id$ */

 /*
   Contributors:
     Created by Reiner Patommel
     Changes: Jochen Pernsteiner, Marek Michalkiewicz
     Changes: Reiner Patommel, 8 Feb 2003
     Changes: Reiner Patommel, 13 May 2003 (DOXYGEN)

   TODO: this implementation uses an inline isspace(). If Avr-libc will
   use locales other than C/POSIX it is needed to call an external isspace().
   
   ATTENTION: an external __mulhi_const_10() function is used: nonstandart
   call conventions: some registers and bit T must be nochanged.
 */

/** \file */
/** \ingroup avr_stdlib
    \fn int atoi(const char *s)
    \brief Convert a string to an integer.
        
    The atoi() function converts the initial portion of the string
    pointed to by \p s to integer representation. In contrast to

        \code (int)strtol(s, (char **)NULL, 10); \endcode

    this function does not detect overflow (\c errno is not changed and
    the result value is not predictable), uses smaller memory (flash and
    stack) and works more quickly.
*/

#if !defined(__DOXYGEN__)

#include "macros.inc"

#define str_hi  r25
#define str_lo  r24
#define num_hi  r25
#define num_lo  r24
#define tmp r18

    ASSEMBLY_CLIB_SECTION
    .global _U(atoi)
    .type   _U(atoi), @function

/*
   Skip leading spaces and tabs.  Process optional sign.  Stop conversion
   on detection of a non-numeric character.  Return 0 if string contains
   no numeric characters. No check is performed whether the value is within
   the range of an 'int' i.e. 32768 becomes -32768.
 */

/* This fact is used below. */
.if ('\t'-9) | ('\n'-10) | ('\f'-12) | ('\r'-13)    ; '\v' is 11
  .err
.endif

_U(atoi):
    X_movw  ZL, str_lo      ; set pointer to string
    CLR num_lo
    CLR num_hi          ; clear number
    CLT             ; clear sign flag

.L_atoi_loop:
    LD  tmp, Z+         ; get (next) character
    CPI tmp, ' '        ; skip whitespace
    BREQ    .L_atoi_loop
    CPI tmp, '\t'       ; ASCII sequence is: \t,\n,\v,\f,\r
    BRLO    1f
    CPI tmp, '\r'+1
    BRLO    .L_atoi_loop
1:
    CPI tmp, '+'        ; if '+' convert
    BREQ    .L_atoi_loop2
    CPI tmp, '-'        ; if '-' remember sign
    BRNE    .L_atoi_digit
    SET             ; remember number is negative
    RJMP    .L_atoi_loop2
    
2:  XCALL   __mulhi_const_10    ; r25:r24 *= 10
    ADD num_lo, tmp     ; num = (num * 10) + (tmp - '0')
    ADC num_hi, __zero_reg__
.L_atoi_loop2:
    LD  tmp, Z+
.L_atoi_digit:
    SUBI    tmp, '0'
    CPI tmp, 10
    BRLO    2b

    BRTC    .L_atoi_done        ; positive number? -> return
    COM num_hi
    NEG num_lo
    SBCI    num_hi, -1      ; make number negative
.L_atoi_done:
    RET

.L_atoi_end:
    .size _U(atoi), .L_atoi_end - _U(atoi)

#endif /* not __DOXYGEN__ */