double fmax(double __x, double __y)
The fmax() function returns the greater of the two values __x and __y. If an argument is NaN, the other argument is returned. If both arguments are NaN, NaN is returned.