void * memmem(const void *, size_t, const void *, size_t) __ATTR_PURE__
The memmem() function finds the start of the first occurrence of the substring s2
of length len2
in the memory area s1
of length len1
.
The memmem() function returns a pointer to the beginning of the substring, or NULL
if the substring is not found. If len2
is zero, the function returns s1
.