8.5 Atmel AVR UC3 OCD
JTAG interface
On some Atmel AVR UC3 devices the JTAG port is not enabled by default. When using these devices it is essential to connect the RESET line so that the AVR Dragon can enable the JTAG interface.
Any stabilizing capacitor connected to the RESET pin must be disconnected when using aWire since it will interfere with correct operation of the interface. A weak external pullup on this line is recommended.
aWire interface
The baud rate of aWire communications depends upon the frequency of the system clock, since data must be synchronized between these two domains. The AVR Dragon will automatically detect that the system clock has been lowered, and re-calibrate its baud rate accordingly. The automatic calibration only works down to a system clock frequency of 8kHz. Switching to a lower system clock during a debug session may cause contact with the target to be lost.
If required, the aWire baud rate can be restricted by setting the aWire clock parameter in the tool-chain. Automatic detection will still work, but a ceiling value will be imposed on the results.
Shutdown sleep mode
Some AVR UC3 devices have an internal regulator that can be used in 3.3V supply mode with 1.8V regulated I/O lines. This means that the internal regulator powers both the core and most of the I/O. The AVR Dragon does not support the Shutdown sleep mode were this regulator is shut off. In other words, this sleep mode cannot be used during debugging. If it is a requirement to use this sleep mode during debugging, use an Atmel AVR ONE! debugger instead.