36.7.33 Preset Value Register

One of the Preset Value Registers is effective based on the selected bus speed mode. The table below defines the conditions to select one of the PVRs.

Table 36-3. Preset Value Register Select Condition
Selected Bus Speed ModeVS18EN

(HC2R)

HSEN

(HC1R)

UHSMS

(HC2R)

Default Speed00don’t care
High Speed0Response Timeout Errordon’t care
Reserved1don’t careOther values

The following table shows the effective Preset Value Register according to the Selected Bus Speed mode.

Table 36-4. Preset Value Registers
PVRxSelected Bus Speed Mode Signal Voltage
PVR0Initialization3.3V or 1.8V
PVR1Default Speed3.3V
PVR2High Speed3.3V

When Preset Value Enable (PVALEN) in HC2R is set to 1, SDCLK Frequency Select (SDLCKFSEL) and Clock Generator Select (CLKGSEL) in CCR are automatically set based on the Selected Bus Speed mode. This means that the user does not need to set these fields when preset is enabled. A Preset Value Register for Initialization (PVR0) is not selected by Bus Speed mode. Before starting the initialization sequence, the user needs to set a clock preset value to SDCLKFSEL in CCR. PVALEN can be set to 1 after the initialization is completed.

Note: Preset Values in PVRx registers are not supposed to be written by the user. However, the user can modify preset values only if Capabilities Write Enable (CAPWREN) is written to 1 in CACR.
Name: PVR
Offset: 0x60 + n*0x02 [n=0..7]
Reset: 0x0000
Property: Read/Write

Bit 15141312111098 
 DRVSEL[1:0]   CLKGSELSDCLKFSEL[9:8] 
Access R/WR/WR/WR/WR/W 
Reset 00000 
Bit 76543210 
 SDCLKFSEL[7:0] 
Access R/WR/WR/WR/WR/WR/WR/WR/W 
Reset 00000000 

Bits 15:14 – DRVSEL[1:0] Driver Strength Select Value for Initialization

Refer to DRVSEL in HC2R.

Bit 10 – CLKGSEL Clock Generator Select

Refer to CGGSEL in CCR.

Bits 9:0 – SDCLKFSEL[9:0] SDCLK Frequency Select Value for Initialization

Refer to SDCLKFSEL in CCR.