44.5.2 Clocks
The TC bus clocks (CLK_TCx_APB) can be enabled and disabled in the Main Clock Module. The default state of CLK_TCx_APB can be found in the Peripheral Clock Masking.
The generic clocks (GCLK_TCx) are asynchronous to the user interface clock (CLK_TCx_APB). Due to this asynchronicity, accessing certain registers will require synchronization between the clock domains. Refer to Synchronization for further details.
Note: Two instances of the TC may share a
peripheral clock channel. In this case, they cannot be set to different clock
frequencies. Refer to the peripheral clock channel mapping of the Generic Clock
Controller (GCLK.PCHTRLm) to identify shared peripheral clocks.