58.2.2 Power Supply Connections
The following figures illustrate the recommended power supply connections for switched/linear mode, linear mode only and with battery backup.
Note:
- VDDIOB is available only on the SG41 device.
Note:
- VDDIOB is available only on the SG41 device.
Note:
- VDDIOB is available only on the SG41 device.
| Signal Name | Associated Ground | Recommended Pin Connection |
|---|---|---|
| VDD | VSS | Capacitors: refer to REG_5 |
| AVDD | AVSS | Capacitors: refer to REG_17 Ferrite Bead(3): Refer to REG_23/REG_25 |
| VDDIOB | VSS |
Capacitors: refer to REG_54(4) |
| VDDCORE | VSS | Capacitors: refer to REG_1 |
| VSW | - | BUCK mode: Inductor required to VDDCORE: Refer
to REG_27/REG_29/REG_31 LDO mode: Not Connected |
| VBAT (PB03) | VSS | Capacitors: refer to REG_13 |
Note:
- REG_X values: Refer to the Power Supply Electrical Specifications from the Electrical Characteristics chapter.
- Decoupling capacitors must be placed close to the device, low ESR capacitors must be used for better decoupling.
- A ferrite bead must be added between the main power supply (VDD) and AVDD to attenuate high-frequency digital noise from entering the analog power domain. The bead must provide enough impedance to help isolate digital and analog power domains. Make sure to select a ferrite bead with a low DC resistance to avoid any relevant IR drop across the ferrite bead that could impact analog peripherals performance.
- The VDDIOB pins are available only on the SG41 devices.
- VDDIOB must be lower or equal to VDDIO and VDDANA.
- When I/O pads in the VDDIOB cluster are multiplexed as analog pads, VDDANA is used to power the I/O. Using this configuration may result in an electrical conflict if the VDDIOB voltage is different from that of VDDIO and VDDANA. If the application has such requirements, it is required to power VDDIOB, VDDIO, and VDDANA from the same supply source to ensure that they are always at the same voltage.