5.1.5 Receiver Blocking and Selectivity Characteristics
This section describes the blocking behavior of the ATA8210/15. The numbers listed are the 3 dB blocking characteristics. The measurements below are carried out with a useful signal at a frequency of fRF and a level of 3 dB above the BER = 10-3 sensitivity levels. For more details, refer to the ATA8210/ATA8215 UHF ASK/FSK Receiver Data Sheet (9344E), section 4, parameter numbers 4.90-5.20. The values indicated describe how much a continuous wave disturber can be larger than these useful signal levels until the BER drops back to 10-3. For example, the sensitivity level is -106.5 dBm, and, at a distance of 1 MHz, the blocking is 64 dBC (see the following figure). For more details, refer to the ATA8210/ATA8215 UHF ASK/FSK Receiver Data Sheet (9344E), section 4, parameter numbers 5.10 and 7.10. The useful signal applied in the measurement is -106.5 dBm + 3 dB = -103.5 dBm and the measured absolute blocker level for BER 10-3 is -103.5 dBm + 64 dBC = -39.5 dBm.
The following figures illustrate the blocking behavior for 433.92 MHz with 165 kHz bandwidth using FSK modulation with a data rate of DR = 20 kBit/s and a frequency deviation of fDEV = ±20 KHZ. See Measured Blocking at ±10 MHz Frequency Offset (fRF = 433.92 MHz, BW = 165 kHz, FSK, DR = 20 kBit/s, fDEV = ±20 kHz) and Measured Blocking in the Frequency Range from 100 MHz to 900 MHz (fRF = 433.92 MHz, BW = 165 kHz, FSK, DR = 20 kBit/s, fDEV = ±20 kHz) in the Receiver Blocking and Selectivity Characteristics from Related Links.
For more details on the differences in the blocking characteristics for other RF or bandwidths, refer to the ATA8210/ATA8215 UHF ASK/FSK Receiver Data Sheet (9344E), section 4, parameter numbers 6.90-7.80. To describe the differences more clearly, the blocking for 25 kHz IF bandwidth and 360 kHz IF bandwidth, see the following figure.
To describe the differences more clearly, the blocking for 25 kHz IF bandwidth and 360 kHz IF bandwidth, see the following figure.