6.1 WILCS02_WINCS02 CLI Example
The WILCS02_WINCS02 CLI is a part of the MCHPRT3 tool installer.
- Double click
MCHPRT3_CLI.exeto run the CLI.Figure 6-1. Command Line Interface - To test the WILCS02_WINCS02, enter the “WILCS02_WINCS02”.
Figure 6-2. Command Line Interface - Enter “Help” to browse CLI help manual.
Figure 6-3. Command Line Interface - For example, enter “StartTx Help” to browse the CLI StartTx Help manual.
Figure 6-4. Command Line Interface
- For example, enter “StartTx Help” to browse the CLI StartTx Help manual.