7.2 Steps to Run the Python 3.11 Environment
The following are the steps to run the Python 3.11 environment:
-
Open IDLE (Python 3.11 32-bit) in the Python 3.11 folder from the PC Start menu.
Figure 7-1. Python IDLE -
The following figure illustrates the “IDLE” window of “Python 3.11”.
Figure 7-2. IDLE -
Go to File > Open and choose the
WILCS02_WINCS02_GUI.pyfile.Figure 7-3. Opening WILCS02_WINCS02_GUI.pyFigure 7-4. Opening WILCS02_WINCS02_GUI.py -
Go to Run>Run Module to execute the
WILCS02_WINCS02.pyfile.Figure 7-5. WILCS02_WINCS02.py -
The “Python 3.11” shell window displays the following message:
Figure 7-6. Check Run WILCS02_WINCS02.pyStatusNote: If the shell window displays an error message, check if the source code is from the originalMCHPRT3_Setup.exeinstallation folder. -
Select the
WILCS02_WINCS02.dllfile to load the library and run the example code.Figure 7-7. WILCS02_WINCS02.dll -
The following figure illustrates the Python shell window. After successfully loading the
WILCS02_WINCS02.dllfile, the Python shell window displays the.dllfile version. In the Python shell window, users can reference the GUI run process to design a tool for themselves.Figure 7-8. Successful Loading of WILCS02_WINCS02.dll -
The following figure illustrates the
WILCS02_WINCS02GUI Python example.Note: Check if the version matches the device HUT code firmware version. -
Select the device connect “COM Port” and click Connect to connect the
WILCS02_WINCS02device.Figure 7-9. Python Example GUI -
The following warning pop-up window appears after connecting the WILCS02_WINCS02 device. Click Yes to Reset the
WILCS02_WINCS02device.Figure 7-10. Warning -
After a successful connection, the following WILCS02_WINCS02 GUI Python example window appears.
Figure 7-11. Python Example GUI