5.1 Gain Table Example
The WILCS02_WINCS02 gain table is a text-based file that can be opened or edited using any text editor. The following rules apply to a gain table file:
- “;;;” indicates a comment for the entire line.
- If the first character is “;”, the row contains file information. Note: Do not modify this row.
- If the first character is blank, the
row contains the Gain Table information. The power target values can be modified,
but no other information or format must be altered.
-
Gain Table information power target values range from 0-25 dBm, with 0.25 dB per step.Note: If any information in the gain table is unavailable, the entire group of information is considered invalid.
Figure 5-1. Gain Table Example
-