6.5.3 fenv Exception Macros
Attention: These macros are implemented only by
MPLAB XC32 C compilers when using a device with a FPU.
The following macros relate to floating-point exceptions.
| Macro | Description |
|---|---|
FE_DIVBYZERO | The operation on finite numbers has produced a result that is infinity. |
FE_INEXACT | The rounded result of an operation differs to the infinite precision result. |
FE_INVALID | The result of the operation cannot be expressed as a value. |
FE_OVERFLOW | The absolute value of the floating-point result is too large to be represented. |
FE_UNDERFLOW | The absolute value of the floating-point result is smaller than the smallest positive normalized floating-point number. |
FE_ALL_EXCEPT | The bitwise OR of the above floating-point exception macros. |