6.5.12 fesetenv Function
Establishes the floating-point environment from an object.
Include
<fenv.h>
Prototype
void fesetenv(fenv_t * envp);
Argument
envp- a pointer to the object in which the environment should be obtained
Remarks
This function establishes the floating-point environment from the object pointed
to by envp. This pointer should be pointing to an object obtained from a call
to fegetenv() or feholdexcept(), or assigned a
floating-point environment macro, such as FE_DFL_ENV. Although the state of
the floating-point status flags are set, these floating-point exceptions are not raised.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <fenv.h>
#include <stdio.h>
int main(void)
{
fenv_t envp;
volatile double x, y=1E30;
fegetenv(&envp); // save the current environment
fesetround(FE_UPWARD); // change the environment
x = 1 / y;
printf("The small result rounded up is %g\n", x);
fesetround(FE_DOWNWARD);
x = 1 / y;
printf("The small result rounded down is %g\n", x);
fesetenv(&envp); // restore the environment
}
Example Output
The small result rounded up is 1.00001e-30
The small result rounded down is 9.99999e-31