5 Appendix B: Running the TCL Script
(Ask a Question)TCL scripts are provided in the design files folder under directory HW. If required, the design flow can be reproduced from Design Implementation till generation of job file.
To run the TCL, perform the following steps:
- Launch the Libero software.
- Select
- Click Browse and select
script.tclfrom the downloaded HW directory. - Click Run.
After successful execution of TCL script, Libero project is created within HW
directory. For more information about TCL scripts, see
mpf_an4592_df\HW\TCL_Script_readme.txt.
For more details on TCL commands, see Tcl Commands Reference Guide. Contact Technical Support for any queries encountered when running the TCL script.