7 Revision History

The revision history describes the changes that were implemented in the document. The changes are listed by revision, starting with the current publication.

Table 7-1. Revision History
RevisionDateDescription
D11/2024The following is the list of changes made in revision D of the document:
C02/2024Added section.
B03/2023Added a note in the Introduction about SmartDebug and API DRI accesses.
A07/2022

The following is the list of changes in revision A of the document:

6.0—Added Appendix B: Running the TCL Script.
5.0—The following is thw summary of the changes made in this revision.
  • Updated the document for Libero SoC v12.2.
  • Removed the references to Libero version numbers.
4.0—Updated the document for Libero SoC v12.1 release.
3.0—Updated the document for Libero SoC v12.0 release.
2.0—Updated the document for Libero SoC PolarFire v2.3 release.
1.0—The first publication of this document.