15.1.2.2 NVM Unlock Sequence
The unlock sequence is a mechanism that protects the NVM from unintended self-write programming or erasing. The sequence must be executed and completed without interruption to successfully complete any of the following operations:
- PFM Row Erase
- Write of PFM write latches to PFM memory
- Write of PFM write latches to User IDs
- Write to Configuration Words
The unlock sequence consists of the following steps and must be completed in order:
Once the WR bit is set, the processor will stall internal operations until the operation is complete and then resume with the next instruction.
Since the unlock sequence must not be interrupted, global interrupts must be disabled prior to the unlock sequence and re-enabled after the unlock sequence is completed.
NVM Unlock Sequence
NVMCON1bits.WREN = 1; // Enable write/erase INTCONbits.GIE = 0; // Disable global interrupts // The next three steps are the required unlock sequence NVMCON2 = 0x55; // First unlock code NVMCON2 = 0xAA; // Second unlock code NVMCON1bits.WR = 1; // Initiate write/erase cycle INTCONbits.GIE = 1; // Enable global interrupts NVMCON1bits.WREN = 0; // Disable further write/erase cycles