5.3.4.6 GenDig - Key Config
In the Key Config mode of the GenDig command,
the slot configuration and key configuration of the key specified by
KeyID are included in the GenDig TempKey calculation. The
Nonce command must be run prior to the first
GenDig command to load a value into TempKey.
Subsequent GenDig commands will use the value from
the previous GenDig operation.
|
Opcode |
Mode |
KeyID(1) |
Data | Description |
|---|---|---|---|---|
| 0x15 | 0x05 | 0x00 0[Slot] | — | Includes slot configuration information |
- KeyId specifies the slot # that will have its configuration information included in the TempKey calculation. The actual slot value is not included.
| Name | Size | Description |
|---|---|---|
| Response | 1 byte |
0x00 - If successful. Error code - If the command fails. |
- TempKey.Valid flag will be set to 1 if successful, otherwise it is 0.
- TempKey.GenDigData will be set to 0.
|
32 bytes |
TempKey.value |