2.6.1 MCC Content Manager

The MCC Content Manager allows users to download versions of supported drivers and libraries for a selected device. The Content Manager for MCC Melody organizes its content into categories such as Libraries, Drivers, System, PLIBs and Examples.

Figure 2-12. Content Manager for MCC Melody
  • The Content Manager for MCC Harmony displays most of its content upfront and categorizes similar items by solutions
Figure 2-13. Content Manager for MCC Harmony
Note:
  1. MPLAB® X IDE users can open the Content Manager before launching MCC by clicking the CM icon on the IDE toolbar.
  2. For VS Code users, the MCC Content Manager can only be accessed from within the MCC Resources panel (refer to the next section).
  3. In MPLAB® X IDE, the MCC Content Manager cannot be opened while MCC is running, as this may result in unexpected behavior or corrupted content.