Save Kit button, which is located on top of the Performance Analyzer
will be enabled if the kit is ready to be saved
When Save Kit button is clicked, a Save As dialog
box will appear
In the Save As dialog box, select any location and choose
a name for the file, and then click Save
Note:
Save Kit will be disabled for
the kits in which the performance application has not yet started.
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.