4.4.2 MatrixMultiply
Description
MatrixMultiply performs the matrix multiplication between the source one and source two matrices and places the result in the destination matrix.
Symbolically:
where:
0 ≤ i < numRows1
0 ≤ j < numCols2
0 ≤ k < numCols1Rows2
Prototype
fractional* MatrixMultiply (int numRows1, int numCols1Rows2, int numCols2, fractional* dstM, fractional* srcM1, fractional* srcM2);
Arguments
|
Parameters |
Description |
|---|---|
|
numRows1 |
Number of rows in the source one matrix. |
|
numCols1Rows2 |
Number of columns in the source one matrix which is same as number of rows in the source two matrix. |
|
numCols2 |
Number of columns in the source two matrix. |
|
dstM |
Pointer to the destination matrix |
|
srcM1 |
Pointer to the source one matrix |
|
srcM2 |
Pointer to the source two matrix |
Returns
Pointer to the base address of the destination matrix.
Remarks
If the absolute value of result in dstM[r][c] is larger than the maximum value of the 1.31 fractional data type, this operation results in saturation for the (r,c)th element.
If the source one matrix is squared, then this function can be computed in place and can be self-applicable.
Source File
- mmul_aa.s
Function Profile
|
Device |
Program Words |
Cycles |
|---|---|---|
|
PIC32A |
27 |
45+numRows1*(6+numCols2*(9+4*(numCols1Rows2 - 1))) |
System resource usage
- W0…W7 - used, not restored
- W8…W12 - saved, used, restored
- ACCA - used, not restored
- CORCON - saved, used, restored
- REPEAT instruction(s) usage – None