5.6.2.1 General
| Option | Description | Command Line1 |
|---|---|---|
| Have symbols in production build | Generate debugging information for source-level debugging in MPLAB® X IDE. | --gdwarf-2 |
| Keep local symbols |
Check to keep local symbols, that is, labels beginning with
Uncheck to discard local symbols. | --keep-locals |
| Preprocessor macro definitions | Project-specific preprocessor macro defines passed via the compiler's
–D option. | -Dmacro[=defn] |
| Assembler symbols | Define symbol sym to a given
value. | --defsym sym=value |
| Preprocessor Include directories | Add a directory to the list of those searched for headers included by the preprocessor. Relative paths are from MPLAB X project directory. | -I dir |
| Assembler Include directories |
Add a directory to the list of those searched for files specified in
You may add as many directories as necessary to include a variety of
paths. The current working directory is always searched first and
then | -Idir |
| Allow call optimization | Turn relaxation on. Convert absolute calls and gotos to relative calls and branches when possible. | --relax |
| Additional driver options | Add driver options not already available in this interface. The string you introduce here will be emitted as-is in the driver invocation command. | |
| ||