Jump to main content
28.4.1.9 Synchronous Host Reception Setup
- Initialize the SPxBRGH:SPxBRGL
register pair and set or clear the BRG16 bit, as required, to achieve the desired baud rate.
- Select the receive input pin by writing
the appropriate values to the RxyPPS and RXxPPS registers. Both selections may enable
the same pin.
- Select the clock output pin by writing
the appropriate values to the RxyPPS and TXxPPS registers. Both selections may enable
the same pin.
- Clear the ANSEL bit for the RXx pin (if applicable).
- Enable the synchronous host serial port by setting the SYNC, SPEN and CSRC bits.
- Ensure that the CREN and SREN bits are cleared.
- If interrupts are desired, set the RCxIE bit of the PIEx
register and the GIE and PEIE bits of the INTCON register.
- If 9-bit reception is desired, set the RX9
bit.
- Start reception by setting the SREN bit or, for continuous
reception, set the CREN bit.
- The RCxIF Interrupt Flag bit will be set when reception of a
character is complete. An interrupt will be generated if the RCxIE enable bit was
set.
- Read the RCxSTA register to get the ninth bit (if enabled) and determine
if any error occurred during reception.
- Read the 8-bit received data by reading the RCxREG
register.
- If an overrun error occurs, clear the error by either clearing
the CREN bit or by clearing the SPEN bit which resets the EUSART.
Figure 28-11. Synchronous Reception (Host Mode,
SREN)