5 Appendix 1: Running the Tcl Script
(Ask a Question)Tcl scripts are provided in the folders of design files under the
directory TCL_Scripts. If necessary, the design flow can be reproduced
from Design Implementation (which includes Synthesis, Place and Route, and Verify Timing)
till the generation of the job file.
To run the Tcl, follow these steps:
- Launch Libero SoC.
- Select
- Click Browse and
select
script.tclfrom the downloadedTCL_Scriptsdirectory. - Click Run.
After successful execution of the Tcl script, a Libero project is created
within the TCL_Scripts directory.
.tcl script
(script.tcl) from shorter paths. It is recommended to download and save
the TCL files closer to the root directory (for example, near the C drive) to ensure a
shorter path.For more information about Tcl scripts, see the
readme.txt at
mpfs_an5165_v2024p1_df/TCL_Scripts.
For more details on Tcl commands, see the Tcl Commands Reference Guide. Contact the Technical Support team for any queries encountered while running the Tcl script.