4.3 Generating the Filter Output
(Ask a Question)To generate the filter output, complete the following steps:
- To configure the input frequencies
and coefficients, click the
icon to connect as shown in the following
figure.Figure 4-5. Connect - After clicking the
icon , the GUI prompts you to press the
SW1 on the board and to click OK
as shown in the following figure.Figure 4-6. Establish Communication - After clicking
OK, click the
icon to start as shown in the following figure.Figure 4-7. Start - After clicking the
icon, the filter operation completes. The GUI displays
the Operation Completed message and plots the filtered data and the
FFT data on the Filter Output tab as shown in the following
figure. As the low-pass filter option was selected, the high-frequency component is
suppressed while the low-frequency signal is preserved. This is observable in the
frequency spectrum of the output signal.Figure 4-8. Filter Output Tab Important: The accuracy of frequencies represented in the frequency plot depends on the frequency resolution used (sampling rate and FFT length). - Zoom-in or zoom-out the waveform
using the options shown in the following figure.
Figure 4-9. Zooming the Filter Output - The Text
Viewer displays the filter coefficients, input signal, output
signal, and FFT output data values, as shown in the following figure.
Figure 4-10. Text Viewer - Close the GUI.
This concludes DSP FIR Filter demo.