4.2.5 Understanding Table Sizes
The stack maintains a set of buffer tables for different functions. CS offers parameters to specify the size of each table. The tables are statically initialized; therefore, these parameters determine the amount of memory allocated at compile time, and, thus, they cannot be configured at run-time. The following table provides details about the configuration parameters that are particularly relevant to the application:
| Table Size Parameter | Description |
|---|---|
CS_NEIB_TABLE_SIZE | Stores information about directly accessible devices from the same network. |
CS_ROUTE_TABLE_SIZE | Stores next-hop addresses for routes towards certain remote nodes if such routes have already been established by route discovery. If the stack fails to find a route in this table, it launches route discovery procedure employing the route discovery table. |
CS_ROUTE_DISCOVERY_TABLE_SIZE | The route discovery procedures use the |
CS_APS_BINDING_TABLE_SIZE | Stores entries for binding links with remote nodes. Each entry contains the source’s extended address and endpoint, as well as the destination’s extended address and endpoint. |
CS_ADDRESS_MAP_TABLE_SIZE | Contains pairs of corresponding short and extended addresses discovered during network operation or by device discovery requests. |
CS_GROUP_TABLE_SIZE | Stores pairs consisting of a group address and an endpoint. Each group address identifies a group that the node is subscribed to, with the endpoint being the destination for data frames addressed to the groups. |
Note: Application developers must properly consider buffer sizes as this can help reduce the amount of Flash memory consumed by the application. | |