4.5.1 Sending a General Cluster Command
To send general cluster commands, use the ZCL_AttributeReq() function with a pointer to an instance of the ZCL_Request_t
type as its argument. The structure behind the pointer includes the following:
- Complete destination specification (device address, destination endpoint, cluster ID and more)
- Command ID
- Source endpoint ID
- Payload length
- Payload itself
In additon, the argument contains the defaultResponse field for
configuring default response bit. Set this field to
ZCL_FRAME_CONTROL_ENABLE_DEFAULT_RESPONSE to ensure that the
destination sends a ZCL default response command, except for commands
that already require a command-specific ZCL response (for example, read
attribute command). A special callback function indicates the reception of
unsolicited default responses.
The following code is an explanation of how to implement the
ZCL_AttributeReq() function with an
example:ZCL_Request_t zclReq; //In the global scope ... zclReq.id = …; // specify command ID, e.g. ZCL_READ_ATTRIBUTES_COMMAND_ID zclReq.endpointId = APP_ENDPOINT_LIGHT; //Source application endpoint zclReq.ZCL_Notify = ZCL_AttributeResp; //The callback function //Setting destination address zclReq.dstAddressing.addrMode = APS_NO_ADDRESS; //Use binding zclReq.dstAddressing.profileId = PROFILE_ID; zclReq.dstAddressing.clusterId = ONOFF_CLUSTER_ID; zclReq.dstAddressing.clusterSide = ZCL_CLUSTER_SIDE_SERVER; //Disable default response (won’t be sent for commands with specific ZCL response) //but can be enabled for requests w/o response (e.g. attribute reports) zclReq.defaultResponse = ZCL_FRAME_CONTROL_DISABLE_DEFAULT_RESPONSE; zclReq.requestLength = …; // specify payload length zclReq.requestPayload = …; // point to payload memory //execute the request ZCL_AttributeReq(&zclReq);
Note: The example does not demonstrate how to populate the
req.requestLength and req.requestPayload
fields. To simplify the process of filling and parsing the payload, as well as
accurately calculating its length, the ZCL component offers the ZCL_PutNextElement() function. Use this utility to ensure these fields
are correctly set within the ZCL_Request_t structure.