5.1.7.3.7 ZCL_PutNextElement Function
Syntax
ZCL_Status_t ZCL_PutNextElement(ZCL_NextElement_t *element);
Description
This function adds an element to the outgoing command payload.
This function enables simplification of the creation of valid payloads for general commands, including reading and writing attributes. A single command can involve actions on several attributes, so the overall payload must contain pieces corresponding to each attribute.
To facilitate the payload, the user must supply a buffer and the associated content. The function, then, performs two critical operations:
- Writes the content in a correct way to the buffer
- Calculates the overall payload length
The function then passes the buffer and the payload length as parameters to the ZCL_AttributeReq() function. The following example code provides more details:
ZCL_NextElement_t element; ZCL_ReadAttributeReq_t readAttrReqElement; ZCL_Request_t readAttrReq; uint8_t buffer[BUFFER_SIZE]; element.payloadLength = 0; element.payload = buffer; element.id = ZCL_READ_ATTRIBUTES_COMMAND_ID; element.content = &readAttrReqElement; readAttrReqElement = ATTRIBUTE_ID1; //Set to the ID of the first attribute ZCL_PutNextElement(&element); readAttrReqElement = ATTRIBUTE_ID2; //Set to the ID of the second attribute ZCL_PutNextElement(&element); readAttrReq.requestLength = element.payloadLength; readAttrReq.requestPayload = buffer; ...
Note: The usage can differ depending on the command’s type.
Input Parameters
| Parameter Name | Description |
|---|---|
element | Information about payload and element [out] status of the operation |
ZCL_SUCCESS_STATUS (0x00) | The system successfully wrote an element to the payload; it can now add more elements. |
ZCL_END_PAYLOAD_REACHED_STATUS (0xFD) | The system wrote an element successfully, and the payload is full; cannot add more elements. |
ZCL_INVALID_PARAMETER_STATUS (0xFF) | The argument is NULL. |
Return Type and Values
- None