5.1.3.3 NWK_GetExtByShortAddress Function
Syntax
const ExtAddr_t* NWK_GetExtByShortAddress(const ShortAddr_t shortAddr);
Description
The function helps in searching a extended address by the short address.
Input Parameters
| Parameter Name | Description |
|---|---|
shortAddr | A short address |
Return Type and Values
- Pointer to the extended address in the address map
- NULL if the extended address is not found