Reading the
AT25080B/AT25160B/AT25320B/AT25640B via the SO pin requires the following
sequence. After the CS line is pulled low to select a device, the
READ (03h) instruction is transmitted via the SI line followed by
the 16‑bit address to be read. Refer to Table 6-6 for the address bits for
AT25080B/AT25160B/AT25320B/AT25640B.
Upon completion of the 16‑bit address, any data on the
SI line will be ignored. The data (D7‑D0) at the specified address
is then shifted out onto the SO line. If only one byte is to be read, the
CS line should be driven high after the data comes out. The
read sequence can be continued since the byte address is automatically incremented and
data will continue to be shifted out. When the highest‑order address bit is reached, the
address counter will roll over to the lowest‑order address bit allowing the entire
memory to be read in one continuous read cycle regardless of the starting address.Figure 6-5. Read Waveform
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.