7 Write Sequence
In order to program the
AT25080B/AT25160B/AT25320B/AT25640B, two separate
instructions must be executed. First, the device must be write enabled via the
Write Enable (WREN) instruction. Then, one of the two possible write
sequences described in this section may be executed.
Note: If the device is not Write Enabled
(
WREN), the device will ignore the WRITE
instruction and will return to the standby state when CS is
brought high. A new CS assertion is required to re‑initiate
communication.The address of the memory location(s) to be programmed must be outside the protected
address field location selected by the block write protection level. During an internal
write cycle, all commands will be ignored except the
RDSR instruction.
Refer to Table 7-1 for the address bits for
AT25080B/AT25160B/AT25320B/AT25640B.| Address | AT25080B | AT25160B | AT25320B | AT25640B |
|---|---|---|---|---|
| AN | A9-A0 | A10-A0 | A11-A0 | A12-A0 |
| Don’t Care Bits | A15-A10 | A15-A11 | A15-A12 | A15-A13 |