3.3.4.1.2 SAM JTAG Pinout (Cortex®-M debug connector)

When designing an application PCB which includes a Microchip SAM with the JTAG interface, it is recommended to use the pinout as shown in the figure below.

Figure 3-9. SAM JTAG Header Pinout
Table 3-5. SAM JTAG Pin Description
Name Pin Description
TCK 4 Test Clock (clock signal from the MPLAB ICD 5 into the target device).
TMS 2 Test Mode Select (control signal from the MPLAB ICD 5 into the target device).
TDI 8 Test Data In (data transmitted from the MPLAB ICD 5 into the target device).
TDO 6 Test Data Out (data transmitted from the target device into the MPLAB ICD 5).
nRESET 10 Reset (optional).
VTG 1 Target voltage reference. Not used by MPLAB ICD 5.
GND 3, 5, 9 Ground. All must be connected to ensure that the MPLAB ICD 5 and the target device share the same ground reference.
KEY 7 Connected internally to the TRST pin on the AVR connector. Recommended as not connected.
Tip: Remember to include a decoupling capacitor between VTG and GND.