33.4.6 Low-Pass Filter Mode
The Low-Pass Filter mode (MD
            = 
        ‘b100) acts
            similarly to the Average mode in how it handles samples; it accumulates samples until
            the CNT value is greater than or equal to RPT, then triggers a threshold comparison. But, instead of a simple average,
            it performs a low-pass filter operation on all of the samples, reducing the effect of
            high-frequency noise on the total, then performs a threshold comparison on the results.
            In this mode, the CRS bits determine the cutoff frequency of the low-pass filter
            (as demonstrated by the Digital Filter/Average section). Refer to the Computation
                Operation section for a more detailed description of the mathematical
            operation.For more information about Low-Pass Filter mode, refer to the
            following Microchip application note, available at the corporate website (www.microchip.com):
    - AN2749, “Using PIC18 12-bit ADC2 in Low-Pass Filter Mode”