3.2.5.2 SPI Distribution
The board features three SPIs (Serial Peripheral Interface). The following schematic shows the SPI distribution.
The serial clock and data lines are shared by the four connected peripherals. Each peripheral has its own dedicated Chip Select line, with one exception, as shown in the table below.
| Peripheral | Interface | Chip Select Number | PIO |
|---|---|---|---|
|
mikroBUS1 |
FLEXCOM4 |
NPCS0 |
PA15 |
|
mikroBUS2 |
NPCS1 |
PA14 | |
|
40-pin RPi connector |
NPCS2 |
PA19 | |
|
40-pin RPi connector |
NPCS3 |
PA20 | |
|
SODIMM connector |
The exception is NPCS3, which is shared between the CS1 line of the RPi connector and the SPI
Chip Select of the SODIMM connector, used to host EDS2 boards. Some EDS2 daughter boards
have SPI communication devices on them.
Warning: If
such a daughter board must be used, make sure not to have an RPi HAT with CS1 loaded
on a device, otherwise a conflict will arise on the bus.