47.5.3 DMA
The DMAC can be configured to use the RX channel of the PCC as trigger source.
If configured, a trigger signal is send to the DMAC when data is received by the PCC, such that the DMAC will automatically read the received data buffer. The buffer ready signal will be automatically clear upon the read done by the DMAC.