ADDR drives the hardware half-word offset from the start address of the corresponding
NVM section when a command is executed using CMDEX. The effective address for the
operation is start address of the SECTION_ADDRESS + 2*ADDR. This register is also
automatically updated when writing to the page buffer.
Example:
For erasing the 3rd row in the Flash memory - spanning from 0x00000200 to 0x000002FF
- ADDR must be written with the half-word offset address of any half-word within this
range, that is any value between 0x100 and 0x17F
Refer to the Physical Memory Map
for more information.