5.17.2 Monitor LLDP-LLDP-MED Neighbors
The LLDP-MED Neighbor Information page provides a status overview of all LLDP-MED neighbors. The displayed table contains a row for each interface on which an LLDP neighbor is detected. This function applies to VoIP devices which support LLDP-MED.

The LLDP-MED Neighbor Information page has the following parameters:
- Interface: The interface on which the LLDP frame was received.
- Device Type: LLDP-MED Devices are comprised of two primary device types: Network Connectivity Devices and Endpoint Devices.
LLDP-MED Network Connectivity Device Definition: LLDP-MED Network Connectivity Devices, as defined in TIA-1057, provide access to the IEEE 802 based LAN infrastructure for LLDP-MED Endpoint Devices. An LLDP-MED Network Connectivity Device is a LAN access device based on any of the following technologies:
- LAN Switch/Router
- IEEE 802.1 Bridge
- IEEE 802.3 Repeater (included for historical reasons)
- IEEE 802.11 Wireless Access Point
- Any device that supports the IEEE 802.1AB and MED extensions defined by TIA-1057 and can relay IEEE 802 frames via any method.
LLDP-MED Endpoint Device Definition: LLDP-MED Endpoint Devices, as defined in TIA-1057, are located at the IEEE 802 LAN network edge, and participate in IP communication service using the LLDP-MED framework. Within the LLDP-MED Endpoint Device category, the LLDP-MED scheme is broken into further Endpoint Device Classes, as defined in the following.
Each LLDP-MED Endpoint Device Class is defined to build upon the capabilities defined for the previous Endpoint Device Class. For-example any LLDP-MED Endpoint Device claiming compliance as a Media Endpoint (Class II) also supports all aspects of TIA-1057 applicable
to Generic Endpoints (Class I), and any LLDP-MED Endpoint Device claiming compliance as a Communication Device (Class III) also supports all aspects of TIA-1057 applicable to both Media Endpoints (Class II) and Generic Endpoints (Class I).
LLDP-MED Generic Endpoint (Class I): The LLDP-MED Generic Endpoint (Class I) definition is applicable to all endpoint products that require the base LLDP discovery services defined in TIA-1057. However, they do not support IP media or act as an end-user communication
appliance. Such devices may include (but are not limited to) IP Communication Controllers, other communication related servers, or any device requiring basic services as defined in TIA-1057.
Discovery services defined in this class include LAN configuration, device location, network policy, power management, and inventory management.
LLDP-MED Media Endpoint (Class II): The LLDP-MED Media Endpoint (Class II) definition is applicable to all endpoint products that have IP media capabilities however may or may not
be associated with a particular end user. Capabilities include all the capabilities defined for the previous Generic Endpoint Class (Class I) and are extended to include aspects related to media streaming. Example product categories expected to adhere to this class include (but are not limited to) Voice/Media Gateways, Conference Bridges, Media Servers, and similar.
Discovery services defined in this class include media-type-specific network layer policy discovery.
LLDP-MED Communication Endpoint (Class III): The LLDP-MED Communication Endpoint (Class III) definition is applicable to all endpoint products that act as end user communication appliances supporting IP media. Capabilities include all the capabilities defined for the previous Generic Endpoint (Class I) and Media Endpoint (Class II) classes and are extended to include aspects related to end user devices. Example product categories expected to adhere to this class include (but are not limited to) end user communication appliances, such as IP Phones, PC-based softphones, or other communication appliances that directly support the end user.
Discovery services defined in this class include provision of location identifier (including ECS/E911 information), embedded L2 switch support, inventory management.
- Capabilities: LLDP-MED Capabilities describes the neighbor unit's LLDP-MED capabilities. The possible capabilities are:
- LLDP-MED capabilities
- Network Policy
- Location Identification
- Extended Power via MDI–PSE
- Extended Power via MDI–PD
- Inventory
- Reserved
- Application Type: Application Type indicating the primary function of the application(s) defined for this network policy, advertised by an Endpoint or Network Connectivity Device. The following are the possible application types:
- Voice: For use by dedicated IP Telephony handsets and other similar appliances supporting interactive voice services. These devices are typically deployed on a separate VLAN for ease of deployment and enhanced security by isolation from data applications.
- Voice Signaling: For use in network topologies that require a different policy for the voice signaling than for the voice media
- Guest Voice: To support a separate limited feature-set voice service for guest users and visitors with their own IP Telephony handsets and other similar appliances supporting interactive voice services
- Guest Voice Signaling: For use in network topologies that require a different policy for the guest voice signaling than for the guest voice media
- Softphone Voice: For use by softphone applications on typical data centric devices, such as PCs or laptops
- Video Conferencing: For use by dedicated Video Conferencing equipment and other similar appliances supporting real-time interactive video/audio services
- Streaming Video: For use by broadcast or multicast-based video content distribution and other similar applications supporting streaming video services that require specific network policy treatment. Video applications relying on TCP with buffering is not an intended use of this application type.
- Video Signaling: For use in network topologies that require a separate policy for the video signaling than for the video media
- Policy: Policy indicates that an Endpoint Device wants to explicitly advertise that the policy is required by the device. Can be either Defined or Unknown
- TAG: TAG is indicative of whether the specified application type is using a tagged or an untagged VLAN. It can be Tagged or Untagged.
- Untagged: The device is using an untagged frame format and as such does not include a tag header as defined by IEEE 802.1Q-2003
- Tagged: The device is using the IEEE 802.1Q tagged frame format
- VLAN ID: VLAN ID is the VLAN identifier (VID) for the interface as defined in IEEE 802.1Q-2003. A value of 1 through 4094 is used to define a valid VLAN ID. A value of 0 (Priority Tagged) is used
if the device is using priority tagged frames as defined by IEEE 802.1Q-2003, meaning that only the IEEE 802.1D priority level is significant and the default PVID of the ingress interface is used instead.
- Priority: Priority is the Layer 2 priority to be used for the specified application type. One of the eight priority levels (0 through 7).
- DSCP: DSCP is the DSCP value to be used to provide Diffserv node behavior for the specified application type as defined in IETF RFC 2474. Contain one of 64 code point values (0 through 63).
- Auto-negotiation: Auto-negotiation identifies if MAC/PHY auto-negotiation is supported by the link partner
- Auto-negotiation Status: Auto-negotiation status identifies if auto-negotiation is currently enabled at the link partner. If Auto-negotiation is supported and Auto-negotiation status is disabled, then the 802.3 PMD operating mode is determined by the operational MAU type field value rather than by auto-negotiation.
- Auto-negotiation Capabilities: Auto-negotiation capabilities show the link partners MAC/PHY capabilities