8.3.2.8 Connection
In this stage, the device shows up in the scan list in the terminal window in order of the following:
IndexMAC AddressDevice name
The following are the steps:
- The script waits for a user to input the
Indexnumber of the desired device from the list to initiate the connection.Figure 8-35. OTAPC using RNBD DFU OTAPC Tool Command Line Execution: Scan Result - Upon receiving the index number, the central device initiates a Bluetooth Low Energy connection with the peer device.
Figure 8-36. OTAPC using RNBD DFU OTAPC Tool Command Line Execution: Connection