5.2.10 Device Information (DINF)

Format: DINF

Use this command to display critical information of the current device over UART. Command D has no parameter.

Example:DINF // Dump information
Response:After issuing command D, the user can see the following information:
  • Device MAC address
  • Device name
  • Connected device – MAC address and address type (public or random) if connected or no if there is no active connection
  • Authentication method – Device I/O capability set by command SA

  • Device features – Device features set by command SR

  • Server services – Bitmap of predefined services that are supported as server role, set by command SS
  • The fixed pin code, if using