4.1 AC Asynchronous Driver

In the Analog Comparator (AC) asynchronous driver, a callback function can be registered in the driver by the application and triggered when comparison is done to let the application know the comparison result.

Summary of the API's Functional Features

The API provides functions to:
  • Initialize and deinitialize the driver and associated hardware

  • Hookup callback handlers on comparison done

  • Enable or disable AC comparator

  • Start single-short comparison if signal-shot mode is enabled (no need to start for continuous mode)

Summary of Configuration Options

Below is a list of the main AC parameters that can be configured in START. Many of these parameters are used by the ac_async_init function when initializing the driver and underlying hardware.
  • Select positive and negative input for AC comparator

  • Select single shot or continuous measurement mode

  • Filter length and hysteresis setting, etc.

  • Run in Standby or Debug mode

  • Various aspects of Event control

Driver Implementation Description

After the AC hardware initialization, the application can register the callback function for comparison done by ac_async_register_callback.

Example of Usage

The following shows a simple example of using the AC. The AC must have been initialized by ac_async_init. This initialization will configure the operation of the AC, such as input pins, single-shot, or continuous measurement mode, etc.

The example registers a callback function for comparison ready and enables comparator 0 of AC, and then finally starts a voltage comparison on this comparator.

          static void ready_cb_AC_0(struct ac_async_descriptor *const descr, const uint8_t comp, const uint8_t result)
          {
              /* Handle date here */
          }
          /**
           * Example of using AC_0 to compare the voltage level.
           */
          void AC_0_example(void)
          {
              ac_async_register_callback(&AC_0, AC_COMPARISON_READY_CB, (ac_cb_t)ready_cb_AC_0);
              ac_async_enable(&AC_0);
              ac_async_start_comparison(&AC_0, 0);
          }
        

Dependencies

  • The AC peripheral and its related I/O lines and clocks

  • The NVIC must be configured so that AC interrupt requests are periodically serviced