66.6.10.1 Input-output Transfer Functions
The ADC can be configured to operate in the following input voltage modes:
- Single-ended—ADC_COR.DIFFx = 0. This is the default mode after a reset.
- Differential—ADC_COR.DIFFx = 1 (see the figure below). In Differential mode, the ADC requires differential input signals having a VDD/2 common mode voltage (refer to section “Electrical Characteristics”).
The following equations give the unsigned ADC input-output transfer function in each mode(1). With signed conversions (see field ADC_EMR.SIGNMODE), subtract 2047 from the ADC_LCDR.DATA value given below.
In the formula, REFP = VREFP, REFN = VREFN.
Single-ended mode:
Differential mode:
If ADC_MR.ANACH is set, the ADC can manage both differential channels and single-ended channels. If ADC_MR.ANACH is cleared, the parameters defined in ADC_COR are applied to all channels.
The following table give s the internal positive and negative ADC inputs assignment with respect to the programmed mode (ADC_COR.DIFFx).
For example, if Differential mode is required on channel 0, input pins AD0 and AD1 are used. In this case, only channel 0 must be enabled by writing a 1 to ADC_CHER.CH0.
| Input Pin | Channel Number | |
|---|---|---|
| Single-ended Mode | Differential Mode | |
| AD0 | CH0 | CH0 |
| AD1 | CH1 | |
| AD2 | CH2 | CH2 |
| AD3 | CH3 | |
| AD4 | CH4 | CH4 |
| AD5 | CH5 | |
| AD6 | CH6 | CH6 |
| AD7 | CH7 | |
| AD8 | CH8 | CH8 |
| AD9 | CH9 | |
| AD10 | CH10 | CH10 |
| AD11 | CH11 | |